Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Optional Features

While the standard insulator is comprised of liquid crystal polymer (LCP), Omnetics also offers more options such as a top latch if the designer's goal is additional retention strength. Hybrid options are also available, encompassing both power (typically found in d-subs) as well as signal contacts. Similar offerings in coax arrangements are also available upon request.

PTM Veröffentlicht am:
PTM Updated on: 2023-03-21