Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
HFR-Slide2

In response to the requirements of high frequency compatibility from the semiconductor tester industry, Omron has developed a differential transmission relay in the 8GHz band within the G6K-RF series. The important features for this market are shown here. It can be used for ATE, various applications using differential transmission methods and other applications requiring higher frequency characteristics.

PTM Veröffentlicht am: