Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Snaps-Slide18

When designing with snap acting switches, it is recommended that no force be applied in the FP. A gap distance of 0.05mm - 1.5mm is recommended with a Total Travel Pushed (TTP) not to exceed the Over Travel (OT) distance. The OT distance is the total distance past the OP (the switched point) of the switch.

PTM Veröffentlicht am: