Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
XN2 Connector Overview Slide 10
Here is an example of a common application for the XN2 e-CON connector providing connection between a ‘Sensor’ and an FA device or semiconductor equipment. These connectors offer an alternate solution for applications currently using ‘Water-proof circular connectors’, ‘Crimp connectors’ and ‘D-SUBs’, which are for external I/O use, indoor, or internal to the appliance, as well.
PTM Veröffentlicht am: