Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
HGS-Slide8

The controller provides a high clarity, 180° visibility, two-line digital display and an intuitive circle meter which displays values between the allowable maximum and minimum values, as indicated by the solid blocks on the unit. The unit allows for the connection of up to fifteen slave units for multipoint calculations. When using multiple fixtures, the unit allows for hot swapping, where the head unit may be removed without powering down the unit.

PTM Veröffentlicht am: