Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
FOV-Slide7

In summary, Panasonic’s "Wide Field of View" passive infrared motion sensor line is an extension to the existing EKMB and EKMC series lineups. Named for their unique capabilities, these passive infrared sensors have a flat and rectangular shape which improves detection in a single axis up to 150°. Also, since the detection zones are overlapping, this sensor can detect motion directly approaching the sensor. Available in white, black, and pearl white.

PTM Veröffentlicht am: