Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List Associated Content
Cost and Volume of Parts

The final criteria for narrowing down a CHO-THERM™ Dielectric Pad would be the customer’s target price and the volume of parts the customer is expecting over a year. Some materials are made entirely in a roll format, which makes them cost effective and good for high volume applications. Those parts are listed above as ‘Higher Volume and Lower Cost Work Cell’. It is worth noting that Boron Nitride ceramic fillers tend to be more expensive. Listed above is a column of dielectric pads with ‘Cost Effective Ceramic Fillers’. Note that both criterion have the same results so the designer has a significant impact on target price and high volume applications if one can use CHO-THERM 1674 or any T441 materials.

PTM Veröffentlicht am: