Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
USB-Switch-Slide22

In summary, Pericom’s USB (universal serial bus) switch has become a dominant interface to fulfill the ever increasing needs for rapid data transfer between end devices such as PC to portable devices, infotainment systems, storage, and GPS, because of its ability to plug and play. USB has effectively replaced a variety of earlier interfaces, such as serial and parallel ports, as well as separate power chargers for portable devices. Pericom’s USB 2.0 products increase device functionality and protect circuitry from accidental damage. USB 3.0 products increase the world’s leading consumer electronics interconnect to a maximum transmission speed of 5Gbps with full-duplex capabilities. Pericom’s USB 3.0 products maintain signal integrity, support independent charging ports, and increase functionality.

PTM Veröffentlicht am:
PTM Updated on: 2015-04-13