Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Features

A nice feature of RIFLINE is that they can be sold as individual components or fully-assembled modules. Ordering as a fully assembled module allows the customer to save time wiring and simplify their bill of materials. The assembled modules are comprised of a base, a relay, a kick-back suppression diode and a retention clip (when applicable) and come equipped with status indication LED. RIFLINE Complete uses all the same accessories as Phoenix Contact’s terminal block line, Clipline Complete, these include the markers, the bridges and the test plug adaptors. Many of the ice-cube relays come with manual operators which can be pushed in to test the contacts briefly or twisted to be toggled into the “active” state.

PTM Veröffentlicht am: