Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
pwr life
Low efficiency causes higher losses, which are emitted in the form of heat. One of the most critical components in determining the life of the power supply is the electrolytic capacitor. Every 10°C rise in temperature reduces the expected lifetime of the capacitor by 50%. Eliminating heat from the capacitors is critical to a long life product, which reduces maintenance efforts and replacement costs.
PTM Veröffentlicht am: