Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
leaf node

The leaf nodes connected to the gateway are the units where the remote sensors and/or the control unit interfaces are located. The physical hardware is very simple and just needs the following parts: the SPR module, the sensors and units to control connected to the SPR module via a local PCB bus, a power source (typically a small battery), the PCB, an antenna (either an external antenna or a PCB antenna), and the enclosure (the mechanical box). This design is very simple to actualize for an electronics engineer with some hardware experience. If a PCB antenna is desired, then an RF designer also needs to be involved.

PTM Veröffentlicht am: