Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
LED-Slide10

In the previous example, a nominal rated forward current of 350mA was used. This is typical for LED lighting applications, but LEDs designed for operation at 700mA, 1A, and even 1.5A are becoming increasingly common. So where the application discussed before requires a 2W resistor rating, higher-powered LEDs may require resistors rated at 10W or possibly even greater.

PTM Veröffentlicht am: