Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Power Resistor Heatsinks Slide 8

In summary, power resistors often require heatsinks to maintain operating temperature. Required thermal resistance needs to be calculated. Finally, there are a few things to consider when working with heatsinks: convection cooling requires thermal grease or pad and proper pressure, heatsink thermal resistance depends on the surface area in contact with ambient air and if the heatsink is too large, a fan can be used or a resistor with a lower thermal resistance can be utilized.

PTM Veröffentlicht am: