Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
BD71847AMWV + i.MX 8M Mini Block Diagram

Shown here is a block diagram of the BD71847AMWV operating with the i.MX8M Mini applications processor. All the rails for the i.MX8M mini can be fully supported by the PMIC. From the SOC and ARM processor to the Memory and GPU, this PMIC has the system fully covered with both the voltage rails required and the correct sequencing needed to properly bring up the system.

PTM Veröffentlicht am: