Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Silicon Carbide (SiC) 4th Generation MOSFET: TO-247-4L Image of ROHM's Silicon Carbide (SiC) 4th Generation MOSFET Switching Loss Diagrams

ROHM’s SiC MOSFET comes in two varieties of leaded TO-247 packages. The latest TO-247-4L package has four leads. The extra lead is dedicated for connecting the gate driver directly to the source of the internal SiC MOSFET. This allows the driver to bypass the parasitic inductance normally encountered at the power source pin. The result is the ability to drive 4-lead SiC MOSFETs at even higher switching speeds, which further reduces switching losses.

PTM Veröffentlicht am: