Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Image of Sanyo Denki Stepper Motor Basics - Basic Step Angle

The basic step angle is the rotation angle per one step. The 2-phase step angle is 1.8°, which means the resolution of the motor is 200 steps per revolution. The 3-phase step angle is 1.2°, which means the resolution of the motor is 300 steps per revolution. The 5-phase step angle is 0.72°, which means the resolution of the motor is 500 steps per revolution.

PTM Veröffentlicht am: