Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Advantages

The ODYSSEY - X86J4105 is more than just a computer; customers can extend up to three SATA with the power connector to build a NAS server. Dual-gigabit Ethernet allows customers to build the OpenWrt project and pfSense with ease. There are also two M.2 PCIe (B-key and M-key), enabling various expandable capabilities including hard drives, SSD, GPU, 4G, and even 5G cellular network connectivity. With the Arduino co-processor onboard, it can be used to connect with sensors and a gyroscope. All these options provide endless possibilities for using the ODYSSEY - X86J4105. Start exploring the IoT journey from here; Seeed has over 300 Grove modules and sensors for customers to choose from.

PTM Veröffentlicht am: