Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Op Modes

The S0MODE bit in the SCON0 register is used to configure the mode of operation. There are two modes available in this particular peripheral. The 8-bit mode and the 9-bit mode. So far, this lecture has covered the 8-bit UART with Variable Baud Rate (Mode 1) and will now look at programming the UART peripheral for 9-bit mode. There are some applications that require multiple UARTs to be connected as a bus. The 9-bit mode is used to signal multiprocessor communications such that the ninth bit gets set to indicate that the data received represents an address. A device with a matching address can accept the data and provide the appropriate action or response. All other devices that don’t have a matching address simply discard the data. The 8-bit mode is the most common mode and is used as the data representation for the RS232 standard.

PTM Veröffentlicht am: