Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
lvpecl
LVPECL is one of the leading differential formats. It provides faster switching speeds by avoiding transistor saturation and has a constant current source driver that results in low noise output, making it ideal for networking and telecom applications. LVPECL has a voltage swing of about 800 millivolts (mV) and the differential cross point is around 2 volts (V). However, LVPECL consumes significantly more power than newer differential output types. The output stage of a driver consists of a pair of NMOS transistors in common source configuration. Typical driver impedance is in the range of 5-Ω to 10-Ω. The Y-Bias termination scheme, shown at the bottom, and the Thevenin termination (not shown here) are popular because resistors are used to set the VDD minus 2 V termination voltage. Other termination schemes are also available.
PTM Veröffentlicht am: