Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
P51-PressureSensors-Slide4

The P51 has excellent linearity and repeatability at better than .1% of span. Linearity is defined as the maximum deviation from a perfect line, depicting output signal change as pressure changes all the way from the minimum pressure to full scale pressure. The full range from the minimum calibrated pressure (usually zero) to the full scale pressure is known as pressure “span”. The ability to be within specification cycle after cycle is known as repeatability.

PTM Veröffentlicht am: