Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
3.4 GH eye 2
HDMI connections transmit data using three transition minimized differential signal (TMDS) pairs. In addition, the TMDS clock pairs as well as DDC clock and DDC data lines which also operate at high speed are transmitted over the cable. These interfaces must be protected with a high speed, low distortion, low loss component such as the ESD/ESDU and ESA/ESAU from Stackpole.
PTM Veröffentlicht am: