Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Latching Form B Reed Relays Overview Slide 9

Applying the nominal voltage to the coil with the proper polarity will fully open the contacts. Care must be taken to make sure the polarity of the coil is maintained so that an opposing field is created negating the magnetic field of the permanent magnet. If the user reverses the coil polarity, the magnetic field of the coil will be aiding the permanent magnet and the contacts will remain closed.

PTM Veröffentlicht am: