Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 12

Several new parameters need to be introduced when discussing RF continuous wave applications and fast digital pulse applications. For RF continuous wave applications the new set of parameters are: insertion loss, isolation, characteristic impedance, VSWR, return loss, and signal to shield impedance. For fast digital pulse applications rise time and slew rate need to be defined. Insertion loss, isolation, and characteristic impedance are also key parameters in the digital world.

PTM Veröffentlicht am: