Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
TG-NSP35 Slide 12

In selecting a product for the automotive industry it is important that it meets a number of stringent requirements for thermal conductivity, mechanical properties, life time and other significant factor. TG-NSP35 has been designed with these criteria in mind and passes all the standard tests. This allows the automotive engineer to specify this material with a degree of confidence. This is critical for the automotive industry where time saving and economics of testing are always major components of the design and qualification process.

PTM Veröffentlicht am: