Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
TG Series Soft Thermal Conductive Pads Slide 15

It is essential that the products are used within the manufacturer’s specified design guidelines. All gap filling materials should be used under compression for optimum thermal performance. Ideally, this should be from 20 – 45% based on the original thickness. This allows the product to wet the surface and form a good interface between the source and the sink. For use outside the parameters stated on the datasheets please contact T-Global directly.

PTM Veröffentlicht am: