Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Epoxy-Slide5

In high-temperature environments, the connectivity reliability is focused on the solder fillet because there are thermal expansion coefficient differences between the substrate, MLCC, and solder fillet. A conductive glue-mounted device allows for more flexibility during periods of expansion and contraction because the thermal expansion differences are reduced by using a non-solder attachment. Conductive glue is a common method of mounting components in applications that demand reliability at high temperatures, particularly in automotive environments. It's also used in applications that cannot be subjected to the heat of the solder paste mounting process. These applications include LCD panels, organic EL and LED displays, and CCD devices, and are particularly sensitive to high temperatures.

PTM Veröffentlicht am: