Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
EMC-Slide21

Though shape and the mounting method is different, clamp filters are a kind of common mode filter. Clamp filters can suppress only common mode noise that flows through interconnecting cables without attenuating the differential mode current as shown in the example above. TDK’s Clamp filters have stable impedance characteristics without any self resonant frequencies while operating at up to 1GHz.

PTM Veröffentlicht am: