Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
highspeed-copper-slide10

The results for the M38999 connector are shown on this slide, with two disconnects in the upper left corner, three in the upper right, followed by four, and five disconnects in the lower left and lower right. As can be seen from the threshold limit lines, two disconnect NEXT is right up against the Gigabit limit line. Although this is considered a pass, there is no headroom with this configuration. As expected, 10 Gigabit Ethernet is not possible (as was previously shown with only one mated pair). Moving onto the groups with three, four, and five disconnects in the link, neither Gigabit nor 10 Gigabit Ethernet speeds are achievable.

PTM Veröffentlicht am: