Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Secrets to a Successful Crimp Slide 5

AWG and wire insulation thickness varies from wire to wire. Just because two wires are listed at the same AWG, it does not mean their insulation thickness is the same. If the user does not take into account both factors the copper or aluminum strands may not fit in the wire barrel correctly, or the terminal’s insulation support may be to large or small for the wire strand.

PTM Veröffentlicht am: