Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
HDO4096-Slide7

Oscilloscope resolution comes from the resolution of the ADC, an ADC has 2N bits of resolution. In an 8-bit system 28 resolution means 256 quantization levels. A 12-bit oscilloscope has 212 resolution or 4096 quantization levels, an improvement of 16 times. This additional resolution enables 12-bit oscilloscopes to display waveforms that are more precise and show more details.

PTM Veröffentlicht am: