Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
High Spped Amplifiers for Video Applications Slide 15

On the left-hand side of this slide, you see the graph from the LMH6715 data sheet. This plot shows what kind of Diff Gain/Diff Phase the LMH6715 is capable of even when driving more than one load or four to be exact in this case. You can see that the Diff Gain/Diff Phase numbers are less than .02% and .02 degrees for all loads shown. On the right, you see the Op Amps produced by TI which meet the requirement of having low Diff Gain/Diff Phase errors with multiple loads.

PTM Veröffentlicht am: