Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
CC3100-CC3200 SimpleLink Wi-Fi Slide 4

The main difference between traditional Wi-Fi and SimpleLink Wi-Fi is the integration of all the SW components (Wi-Fi driver, Supplicant, TCP/IP, and SSL ) into the SimpleLink device – which significantly reduces the MIPS and Memory requirements from the Host MCU and allows for a low power solution. Using the SimpleLink Wi-Fi devices, an embedded product can be connected securely to the Internet.

PTM Veröffentlicht am: