Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Circuit Isolation Techniques Slide 9

Shown on this slide are several isolation techniques; capacitive, inductive, GMR, and optical. The question is which of these is capacitively coupled? The correct answer is E. All of these devices and techniques are capacitively coupled. Only the capacitive based isolation takes this and leverages it as a strength, whereas the others view it as more of a parasitic parameter.

PTM Veröffentlicht am: