Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Dual-Mode Bluetooth Slide 8

The MODN offers dual-mode Bluetooth 4.1 with a transmit power of 10 dBm and receive sensitivity of -93 dBm. This evaluation module (EM) is fully certified for FCC, IC for Canada, and CE for Europe and comes with a royalty free Bluetooth stack. The available software for the MODN runs the Bluetooth profiles and stack on an external host MCU such as MSP430 or TM4C that connects to the module through a UART connection. The module with the integrated antenna, MODA which will be coming soon, offers the same capabilities as the MODN with a software stack that runs on an external host with the UART connection. The MODA packaging is similar to the MODN except for the size because of the integrated antenna, which is where the MODN and MODA differ. Customers would also not have to worry about antenna design along with being able to make use of the FCC/CE/IC certification available on the module.

PTM Veröffentlicht am: