Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
ISOW7841-Slide11

The ISOW7841 emissions performance is shown on this slide. On the left side, one can see the ISOW7841 radiated emissions data, indicated by the green line, with the CISPR22 class B line in blue. As seen in the image, the ISOW7841 passes the class B emissions standard. On the right side, the same CISPR22 standard is shown along with the emission profile of the competitor’s device, the red line. As is evident from this image, the competitor’s device does not meet the CISPR22 standard. The ISOW7841 offers 10dB lower radiated emissions compared to the competitive device which improves system signal integrity by minimizing system noise. In addition, it provides robust EMC to meet IEC61000-4-X standards for ESD and EFT events, helping to ensure reliable operation of the system. Finally, the ISOW7841 has a high level of immunity which helps reduce the effect of noise and high-voltage events on industrial equipment.

PTM Veröffentlicht am: