Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Topic 5 The Analog Subsystem Slide 4

This slide shows a more detailed overview of the F28M35x. Note the distinctiveness of the master system, which is the Cortex-M3 CPU and the default system at boot, and the control system, which is the C28X CPU. But both of these systems, even though they share a memory and run their individual code in their individual flash banks, share the ADC and both have access to the ADC. The key thing to keep in mind is that as with all C2000 devices, the control system is at the heart of that device. The C28X accessing the ADC is a critical part of having a successful control system.

PTM Veröffentlicht am: