Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Inter-Processor Communications Slide 9

To enable IPC through the peripherals there is a mode called serial port loopback. This mode supports UART to SCI as well as SSI to SPI. The master subsystem can enable or diable this capability. Furthermore, it does not require an external connection between the peripherals. Note that the pins can also be seen on the GPIOs when in this mode, which may be useful for debug.

PTM Veröffentlicht am: