Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
IPC Part 2 Slide 18

In summary, there are three software options to choose from when implementing inter-processor communication on a Concerto MCU. The first, and simplest, is basic IPC, which communicates via message RAMs and shared SARAM blocks along with IPC flag registers. Its simplicity makes it a good option for basic applications, though it is comparatively limited in functionality. The IPC-Lite drivers solution is the next step up in complexity and is the option likely to be ideal for most customers. It includes basic functions for manipulating 16 to 32-bit words; including read/write, calling functions on the other processor, and so on. It additionally retains a measure of simplicity in that it requires no additional setup in the application code. The Main IPC Drivers solution is the third and final software option for IPC. This is a full featured option and includes features such as a circular buffer for queuing up multiple commands as well as all features offered in previous options. It is the most complex and requires additional setup in the application code.

PTM Veröffentlicht am: