Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
The Ultra Low Power MSP430 Slide 14

Internal peripherals can also be power managed for effective current consumption. Here an example is shown using the on-chip comparator of the MSP430F20x1 devices to quickly check an external sensor’s value. The current consumption for this comparator is roughly 45 microamps. In this case, the desire is to power up the comparator, check its status and disable it as soon as possible. Please note that the resistor divider made from the sensor is powered from a port pin allowing direct control over powering the resistor divider, further reducing current consumption.

PTM Veröffentlicht am: