Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Powering FPGAs Slide 11
In this example, the bode plot shows the crossover frequency is much higher at 36 kilohertz. The over and undershoot excursions are much less by nearly 50% from the previous example. Phase margin is at 48 degrees, which is less than what it was on the previous slide, but the regulator is still critically damped.
PTM Veröffentlicht am: