Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
How to Select a Tripp Lite PDU Slide 16

Tripp Lite Dual-Circuit PDUs are like having two PDUs in one housing. It features two separate input power circuits with corresponding, color-coded (black and gray) power cords, circuit breakers, outlets, and (if applicable) current meters. Dual-Circuit PDUs are designed to accommodate the two, redundant input power cords found on most mission-critical network devices. Using the PDU's two separate circuits, managers can build a fault-tolerant rack installation by sourcing power from two separate power sources. Depending on the desired level of power protection, the two sources can be two UPS systems, two generator-supported utility wall outlets or one UPS system and one generator-supported utility wall outlet. Since PDUs with dual input circuits consolidate the features of two models into one housing, it reduces clutter and allows for increased airflow in racks.

PTM Veröffentlicht am: