Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
How to Select a UPS System Slide 13

The National Electrical Manufacturer's Association (NEMA) has developed standards for input (plugs) and output (receptacles) to ensure that end users do not accidentally connect devices to power sources with incompatible voltages and amperages--which could create dangerous conditions. The blade type, voltage and amperage of a plug must match the blade type, voltage and amperage of a receptacle. For example: "L" (twist lock) plugs can only be used with "L" (twist lock) receptacles; "5" (120 V) plugs can only be used with "5" (120 V) receptacles; "20" (20 A) plugs can only be used with "20" (20 A) receptacles. Note: there are only two receptacles (5-15/20R and 6-15/20R) that are designed to accept both 15- and 20-amp plugs. 5-15/20R receptacles accept both 5-15P and 5-20P plugs. 6-15/20R receptacles accept both 6-15P and 6-20P plugs. There are no other exceptions.

PTM Veröffentlicht am: