Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
IntegratedConnector-Slide14

In an ICM, the magnetics are shielded, which prevents any RF coupling onto the magnetic wires and provides better EMI attenuation. It is advantageous to keep the traces from the PHY to RJ-45 as short as possible. Traces have a tendency to act like antenna, thereby diminishing a systems EMI performance. Since it is possible to keep trace lengths much shorter with these solutions, the overall system EMI performance is optimized.

PTM Veröffentlicht am: