Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
PSM Series: Target Applications

The PSM series is targeted for applications in the consumer space such as virtual reality and headset volume control. These products are also targeted at pro-audio applications such as audio mixing boards and volume controls. The PSM can also be utilized in medical or dental position sensing applications and nearly any control panel, such as an industrial welder or mobility scooter panel controls, in the transportation and industrial markets.

PTM Veröffentlicht am: