Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Conceptual Model of Castle Patch Antenna

Unictron will design the structure of the castle, based on the spec that the customer needs. For example, castle 3010, is based on the customer’s spec that needs L1+L5 frequencies, the dimension is 30 * 30 mm, and the height has to be 10 mm. This conceptual model makes the customer understand the combination of castle structure.

PTM Veröffentlicht am: