Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List Associated Content
Image of Vishay BC Components PTCEL Thermistors - Resistance

The safety feature of the PTCEL is the exponential change in resistance with small change in temperature once temperature passes the switch temperature. If there is a short-circuit failure, the internal I2R losses will cause the PTC to heat up to high resistance quickly. The result is a very small residual current. The PTC will remain at high resistance until the energy source is removed and the PTC cools down below the tripping temperature.

PTM Veröffentlicht am: