Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
ESD Protection Family Slide 8

This portion of the Vishay ESD portfolio has two functionalities. One is ESD protection and clamping, the second is EMI filtering. This combination makes good sense because many applications are very sensitive to EMI and ESD at the same input ports, therefore they work together at the same place. The simulation circuit shows the function of clamping the strike, and filtering the RF.

PTM Veröffentlicht am: