Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Markings

The RCM series resistors offer a significant improvement when it comes to traceability of leaded metal film resistors, using detailed markings that clearly show the series name, size, ohmic value (in Ω), tolerance (in %), temperature coefficient, and manufacturing date code. This is a significant improvement over traditional color-coded bands which only represent the resistance value but give no indication of the manufacturer, series, resistance tolerance, temperature coefficient, or date code. Here, users can see an example of the RCMT series high temperature style, with the date code definitions shown in the table to the right.

PTM Veröffentlicht am: