Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Non-Magnetic MLCCs Slide 6

The magnetic field generated by an MRI will attract ferromagnetic objects with considerable force. This attraction is usually referred to as the "missile effect" and poses a significant risk to anyone in or near the unit. Serious injuries can be caused to patients when a ferromagnetic object is pulled into the MRI magnet core. These objects include oxygen bottles, chairs, ladders, carts, pens, and scissors.

PTM Veröffentlicht am: