Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
UHF Chip Antenna Slide 10

To visualize how it works, assume the digital inputs are set both to High level. In this state, both PIN diodes conduct and the total impedance will be dictated by L1 and C2. The antenna will be tuned as shown. The antenna Bandwidth is ~ 100MHz, so several channels can be tuned in this portion of the UHF spectrum.

PTM Veröffentlicht am: